In the world of chemical and petrochemical processing, there’s no room for error. These operations run around the clock, handling high temperatures, high pressures, and high stakes. Whether it’s refining crude oil, producing industrial chemicals, or manufacturing plastics, temperature control is absolutely critical.
That’s where intercoolers and subcoolers come in.
They may not always get the spotlight, but these components are the quiet workhorses keeping processes safe, efficient, and productive.
At Genemco, we know how important it is to have equipment that performs when it matters most. That’s why we offer a wide selection of quality used intercoolers and subcoolers from trusted names like E.L. Nickell Co., RVS, RECO, FES, Frick, Vilter, and many more. If you're upgrading or expanding your facility, Genemco is your go-to for reliable, high-performance cooling solutions.
Image from Genemco
Link to Intercoolers and Subcoolers
The Role of Intercoolers in Chemical & Petrochemical Operations
In chemical plants and refineries, gases are often compressed in multiple stages. These gases heat up rapidly during compression, which can stress the system, reduce performance, and even become dangerous.
Intercoolers help solve this problem by cooling the gas between each compression stage. This improves safety, extends the life of compressors, and boosts energy efficiency.
You’ll find intercoolers at work in:
-
Hydrogen, nitrogen, or natural gas compression
-
Ammonia production
-
Polymer and plastic synthesis
-
Gas dehydration and separation processes
Intercoolers not only help systems run smoother—they also help facilities meet environmental and safety standards more easily.
Subcoolers: Supporting Critical Temperature-Sensitive Reactions
Subcoolers, on the other hand, focus on optimizing the refrigerant side of cooling. By lowering the temperature of liquid refrigerant below its condensation point, subcoolers ensure better heat absorption and higher efficiency within chilling systems.
In the chemical industry, this plays a big role in:
-
Condensing volatile vapors
-
Stabilizing reaction temperatures
-
Improving performance of closed-loop refrigeration systems
-
Preventing premature vaporization in chillers
For example, in a petrochemical plant separating hydrocarbon fractions, precision cooling is key to product purity. A well-functioning subcooler ensures that systems maintain tight control over process temperatures—even in high-demand environments.
Real-World Value in Harsh Environments
Chemical and petrochemical plants operate in some of the harshest conditions. Equipment needs to be tough, dependable, and energy-efficient. That’s why so many companies turn to used equipment from Genemco—because it performs, without the new-equipment price tag.
Image from Genemco
Link to Intercoolers and Subcoolers
Why Genemco?
We’ve spent decades helping plants across the U.S. and beyond find the right equipment to stay productive and competitive. Whether you’re replacing a failed unit or expanding a line, we make the process simple—and affordable.
When you shop with Genemco, you get:
-
Access to top brands like Frick, FES, E.L. Nickell Co., RVS, RECO, and Vilter
-
Personalized support from a team that understands your industry
-
Equipment that’s ready to ship when you need it most
Ready to Upgrade or Expand?
Don’t let a failed equipment slow your plant down. At Genemco, we help chemical and petrochemical companies stay ahead with dependable cooling equipment—without the long lead times or inflated costs.
👉 Browse our inventory at Genemco.com, or reach out to our team. We’re here to help you find the right intercooler or subcooler for your process—quickly, confidently, and cost-effectively.