A Cleaner Process, From Start to Finish: Ozone Systems in Food & Beverage Water Treatment

In food and beverage processing, water touches almost everything—your product, your equipment, your reputation. Whether it’s rinsing fresh produce, sanitizing processing lines, or circulating through cooling systems, water quality isn’t just a utility concern—it’s a production priority.

That’s why more facilities are turning to ozone systems as a smarter, more efficient way to treat water without introducing additional chemicals into the process.

Let’s take a closer look at how ozone works in this environment—and why it’s becoming a go-to solution across the industry.

Image from Genemco
Link to Ozone Systems

What Is an Ozone System in Water Treatment?

An industrial ozone system is designed to generate ozone gas (O₃) on-site and inject it directly into water streams for treatment.

In food and beverage applications, this process typically involves:

  • An ozone generator (creating ozone from oxygen)
  • A contact system (where ozone dissolves into water)
  • Destruct units (to safely break down excess ozone gas)

Once dissolved, ozone gets to work immediately—oxidizing contaminants, neutralizing microorganisms, and breaking down organic matter.

The key advantage?
It does all of this without leaving behind chemical residues that could affect product quality or require additional rinsing steps.

Where Ozone Fits in Food & Beverage Processing

Unlike traditional disinfectants, ozone is versatile enough to be used across multiple stages of production. It’s not just a “one-point solution”—it’s integrated throughout the process.

Produce Washing & Surface Sanitation

Fresh fruits and vegetables are highly susceptible to microbial contamination.

Ozone-treated water helps:

  • Reduce pathogens like E. coli and Salmonella
  • Extend shelf life
  • Maintain product integrity without chemical taste or residue

Meat, Poultry & Seafood Processing

Sanitation is critical in protein processing environments where contamination risks are high.

Ozone is used to:

  • Wash carcasses and cuts
  • Sanitize conveyors and contact surfaces
  • Control odors in processing areas

Clean-in-Place (CIP) Systems

Ozone can be integrated into CIP systems to sanitize tanks, piping, and fillers.

Benefits include:

  • Reduced reliance on harsh chemicals
  • Lower water consumption (less rinsing required)
  • Faster turnaround between production runs

Beverage & Bottling Operations

From bottled water to soft drinks and breweries, ozone plays a key role in maintaining purity.

Common uses:

  • Bottle and container rinsing
  • Ingredient water treatment
  • Microbial control without altering taste profiles

Cooling Towers & Refrigeration Support Systems

Water used in cooling systems can quickly become a breeding ground for biofilm and bacteria.

Ozone helps:

  • Keep systems cleaner
  • Improve heat exchange efficiency
  • Reduce maintenance and chemical dosing

For teams managing industrial refrigeration, that means fewer headaches and more consistent performance.

Why Food Processors Are Moving Toward Ozone

For operations teams balancing food safety, efficiency, and cost control, ozone checks a lot of boxes:

  • Residue-Free Sanitation: Breaks down into oxygen—no chemical carryover
  • Strong Oxidation Power: Effective against a broad spectrum of microorganisms
  • Operational Efficiency: Reduces water usage and cleaning cycle times
  • Product Integrity: Doesn’t impact flavor, color, or texture
  • Regulatory Alignment: Accepted for use in food processing applications

In short, it simplifies sanitation without compromising standards.


Image from Genemco
Link to Ozone Systems

When Timing Isn’t on Your Side—Where Genemco Comes In

Even when ozone is the right solution, getting a new system installed isn’t always immediate.

Lead times can stretch. Projects can stall. And production? It doesn’t pause.

That’s where Genemco becomes a practical partner.

Supporting OEMs—Not Competing With Them

If you’re an OEM working with a customer on a new ozone system, we’re not here to step on that relationship.

We want you to win that project.

But if your customer is stuck waiting—weeks or months—for new equipment, that gap can be costly. Downtime, reduced output, or temporary workarounds all add up.

Genemco can step in with available equipment to help bridge that gap.

Think of it as:

  • A short-term solution to maintain operations
  • A “bandaid” or “tourniquet” to keep production moving
  • A way to support your customer until your system is installed

When your equipment arrives and goes live, you’re still the one who delivered the long-term solution.

Why Teams Turn to Genemco

  • Ready-to-Ship Inventory: When waiting isn’t an option
  • Budget Flexibility: Cost-effective alternatives for temporary needs
  • Industry Familiarity: We understand the realities of food processing and refrigeration environments
  • Real Solutions, Fast: Not theory—practical equipment that keeps plants running

The Bottom Line

Ozone systems are changing the way food and beverage facilities approach water treatment—offering a cleaner, faster, and more efficient path to sanitation.

But even the best systems don’t eliminate the challenges of timing, logistics, and unexpected downtime.

That’s where having the right partner matters.

Genemco isn’t here to replace your long-term plans—we’re here to support them. To help you keep things moving when the clock is working against you. And to make sure that when your full solution is in place, your operation—and your reputation—never skipped a beat.