When most people hear the words cryogenic processing, they probably don't immediately think about heat exchangers. But for the people who design, operate, and maintain these systems, heat transfer is at the heart of the process.
Whether you're separating air into oxygen and nitrogen, processing natural gas, recovering helium, or working with liquefied gases, getting a process stream to the right temperature—and keeping it there—is critical.
That's where plate-fin heat exchangers have earned an important place in the cryogenic and natural gas industries.
Their compact construction, high heat-transfer surface area, and ability to handle multiple streams make them particularly useful in applications where temperatures can drop to levels far below what most industrial equipment ever encounters.
And when you're working at cryogenic temperatures, "close enough" isn't usually good enough.
Image from Genemco
Link to Plate-Fin Heat Exchangers
What Makes Plate-Fin Heat Exchangers Well Suited for Cryogenic Applications?
A plate-fin heat exchanger is built from alternating layers of plates and corrugated fins. The plates separate the different fluid streams, while the fins create flow passages and greatly increase the available surface area for heat transfer.
The result is a compact heat exchanger capable of transferring significant amounts of heat without requiring a massive footprint.
For cryogenic applications, that's a big advantage.
Many cryogenic systems need to move heat between several process streams while maintaining extremely small temperature differences. A plate-fin exchanger can be designed to accommodate multiple streams within the same core, allowing engineers to integrate several heating and cooling duties into one piece of equipment.
Brazed aluminum plate-fin heat exchangers are especially common in cryogenic service because aluminum has favorable thermal properties at very low temperatures.
But perhaps the biggest benefit is heat recovery.
In a cryogenic plant, one stream may be extremely cold while another is relatively warm. Instead of allowing that cold energy to go to waste, the exchanger can transfer it to an incoming stream that needs to be cooled.
The process essentially gets more mileage out of the energy already in the system.
Plate-Fin Heat Exchangers in Cryogenic Processing
Cryogenic processing covers a surprisingly broad range of industries and applications. What they have in common is the need to operate at extremely low temperatures and maintain carefully controlled thermal conditions.
Here are some of the areas where plate-fin heat exchangers are commonly used.
Air Separation
Air may seem simple enough, but separating its major components on an industrial scale is a highly engineered process.
Air separation units, or ASUs, use cryogenic processes to separate atmospheric air into products such as oxygen, nitrogen, and sometimes argon.
The air is first compressed, cleaned, and cooled before being separated through cryogenic distillation.
Plate-fin heat exchangers play an important role in the cooling and heat-integration side of the process.
Incoming compressed air needs to be cooled to cryogenic temperatures, while product streams leaving the distillation process are extremely cold.
A plate-fin exchanger can transfer heat between those streams, using the cold product gases to precool incoming air.
That means the system isn't simply throwing away all of that valuable cold energy.
Instead, it can be recovered and reused.
For a continuously operating air separation plant, that heat integration can be an important part of the overall process efficiency.
Oxygen Production
Industrial oxygen is used across industries including steelmaking, healthcare, chemical processing, water treatment, and manufacturing.
One major method of producing high-purity oxygen is cryogenic air separation.
During the process, air is cooled until it reaches temperatures where its components can be separated based on their different boiling points.
Plate-fin heat exchangers help provide the necessary cooling and warming of process streams throughout the system.
Because oxygen production involves extremely cold temperatures, efficient heat transfer is essential. The exchanger can help precool incoming air and warm outgoing oxygen and nitrogen streams while recovering refrigeration from those cold product streams.
The result is a highly integrated thermal system in which streams entering and leaving the process can exchange energy with one another.
Nitrogen Production
Nitrogen is another major product of cryogenic air separation.
It's used in everything from food packaging and chemical processing to electronics manufacturing, pharmaceuticals, inerting, and industrial refrigeration.
Cryogenic nitrogen production requires the air to be cooled to extremely low temperatures so that oxygen, nitrogen, and other components can be separated.
Plate-fin heat exchangers are well suited for this environment because they can efficiently transfer heat between multiple streams while occupying relatively little space.
For example, cold nitrogen leaving the separation process can be used to cool incoming air.
That might sound like a simple concept, but in a large industrial system operating continuously, recovering that cold energy can be extremely valuable.
Hydrogen Processing
Hydrogen processing is another area where cryogenic heat transfer can become important.
Hydrogen can be processed, purified, separated, compressed, and liquefied depending on the application. Some processes require extremely low temperatures, particularly when hydrogen is being liquefied.
Plate-fin heat exchangers can be used to provide cooling and heat recovery within hydrogen processing systems.
Hydrogen liquefaction is particularly demanding because hydrogen must ultimately be cooled to approximately -423°F (-253°C) to become a liquid at atmospheric pressure.
At those temperatures, every stage of the thermal process matters.
Plate-fin technology can provide the high surface-area heat transfer needed to progressively cool process streams while keeping the equipment relatively compact.
Helium Recovery & Liquefaction
Helium is one of the more unusual applications for cryogenic processing.
Because helium has an exceptionally low boiling point, recovering and liquefying it requires temperatures close to absolute zero compared with most industrial processes.
Plate-fin heat exchangers can be incorporated into helium recovery and liquefaction systems to provide highly efficient heat transfer between extremely cold process streams.
In these systems, recovering refrigeration from outgoing streams is particularly important.
The colder a process gets, the more carefully engineers have to manage every bit of available refrigeration.
A well-designed heat exchanger becomes more than simply a piece of equipment that "moves heat." It becomes part of the overall refrigeration strategy.
Liquefied Gas Processing
Cryogenic systems aren't limited to oxygen, nitrogen, hydrogen, and helium.
Plate-fin heat exchangers are also used in the processing of liquefied gases and in applications involving natural gas and other hydrocarbon streams.
Natural gas processing and LNG systems are particularly notable examples.
LNG stands for Liquefied Natural Gas.
Natural gas is cooled to approximately -260°F (-162°C) so that it changes from a gas into a liquid. Liquefying the gas dramatically reduces its volume, making it practical to store and transport by specialized LNG carriers.
Plate-fin heat exchangers can be incorporated into the refrigeration and liquefaction process to transfer heat between natural gas and refrigerant streams and to recover cold energy from streams leaving the process.
Their compact design and ability to handle multiple streams make them a natural fit for highly integrated cryogenic systems.
Natural Gas: Another Place Plate-Fin Technology Shines
The relationship between plate-fin heat exchangers and cryogenic processing extends well beyond LNG liquefaction.
Natural gas processing facilities may use cryogenic temperatures to help separate valuable components from the incoming gas stream.
Depending on the process, plate-fin heat exchangers can be involved in applications such as:
- Gas cooling
- Gas-to-gas heat recovery
- NGL recovery
- Nitrogen rejection
- Cryogenic separation
- LNG production
- Refrigeration and precooling
In many of these applications, the exchanger isn't working alone. It's part of a much larger thermal system where compressors, expanders, separators, refrigeration systems, and other equipment all have to work together.
That's why selecting the right heat exchanger isn't simply a matter of finding one with the right dimensions.
The process, fluid, pressure, temperature, flow rate, materials, and configuration all matter.
Why Compactness Matters in Cryogenic Plants
One of the biggest advantages of plate-fin heat exchangers is their ability to provide a lot of heat-transfer surface in a relatively small package.
And in cryogenic processing, that's more than a convenience.
Large industrial gas facilities contain an enormous amount of equipment. Compressors, towers, vessels, piping, pumps, controls, refrigeration systems, and heat exchangers all have to fit together into a functioning plant.
If engineers can achieve the required heat transfer in a smaller package, it can provide valuable flexibility in the overall plant design.
The same compactness that makes plate-fin heat exchangers attractive from an engineering perspective can also make them useful when replacing existing equipment where space is already limited.
Finding the Right Equipment Doesn't Always Mean Buying New
Here's the reality of industrial equipment: sometimes the equipment you need today isn't the equipment you ordered six months ago.
A new cryogenic heat exchanger can involve engineering, fabrication, testing, transportation, installation, and commissioning. Depending on the application, that can mean a significant lead time.
But the process may not have the luxury of waiting.
An existing exchanger could fail. Production requirements could increase. A project could get accelerated. A customer could need a temporary solution while the permanent equipment is being manufactured.
That's where pre-owned equipment can provide another option.
At Genemco, we specialize in pre-owned industrial refrigeration and food processing equipment, giving customers access to equipment that is already available rather than always starting with a new-build order.
For specialized equipment like plate-fin heat exchangers, availability and application fit are important. The goal isn't simply to find something that looks similar.
It's about evaluating whether an available piece of equipment can make sense for the intended application.
Image from Genemco
Link to Plate-Fin Heat Exchangers
Genemco: Helping Bridge the Gap
Genemco's experience in the used industrial equipment market can be particularly helpful when you're trying to solve an equipment problem under a deadline.
Our inventory changes, which means the equipment available today may not be the same equipment available next month.
That can be an advantage when a project needs something sooner than a new manufacturing schedule allows.
Whether you're looking for a heat exchanger for a replacement application, a temporary system, additional capacity, or equipment to keep a project moving while new machinery is being built, Genemco can help you explore the pre-owned market.
And sometimes that's exactly what a project needs.
Not necessarily the final solution.
Just the solution that keeps things moving until the final solution arrives.
OEMs: We Want to Help You Keep Your Customer
If you're an OEM, we understand that your relationship with the customer comes first.
You've made the sale. You've engineered the solution. Your customer is counting on you to deliver.
The last thing we want to do is get in the middle of that relationship.
We want to help you make the sale work.
Let's say you've sold a new heat exchanger or cryogenic system, but the equipment has a long lead time.
Your customer still has a plant to operate.
Rather than asking them to simply wait, consider Genemco as a resource for a temporary or interim equipment solution.
Think of us as the bandaid that gets the operation through a short-term problem—or, if things are more serious, the tourniquet that helps keep the operation alive until the permanent solution is ready.
You don't lose the customer.
You don't lose the sale.
And your customer doesn't have to sit idle waiting for the new equipment.
You remain the hero.
Genemco simply helps fill the gap.
When the new equipment arrives, your permanent solution can take over as planned.
That's the kind of relationship we want with OEMs: you bring the long-term solution, and we help you keep the customer running in the meantime.
When Every Degree Matters
Cryogenic processing operates in a world where temperatures are extreme, processes are interconnected, and efficiency matters.
From air separation and oxygen production to nitrogen, hydrogen, helium, LNG, and other liquefied gas applications, plate-fin heat exchangers can play a critical role in moving heat—and recovering cold—throughout these systems.
They're compact. They're efficient. They can handle multiple streams. And they're capable of operating in some of the coldest industrial environments on Earth.
But even the best equipment doesn't help much if it's sitting in a factory waiting to be built while your customer's process is down.
That's where Genemco comes in.
When the permanent equipment is on the way but the operation can't wait, we're here to help find a bridge between the two.
Because sometimes keeping an operation running isn't about finding the perfect long-term answer.
It's about finding the right answer right now.