In wastewater treatment, the finish line matters just as much as the process itself. By the time water is ready for discharge—or reuse—it has to meet strict regulatory standards while still being handled efficiently and cost-effectively.
For many facilities, especially those tied to food processing and industrial operations, traditional treatment methods can only go so far. Trace contaminants, residual organics, and microbial risks don’t always respond easily to conventional approaches.
That’s where ozone systems step in—not as a replacement for your entire treatment process, but as a powerful final layer of protection and polish.
Image from Genemco
Link to Ozone Systems
What Is an Ozone System in Wastewater Treatment?
In wastewater applications, an ozone system generates ozone gas (O₃) on-site and introduces it into treated water—typically toward the final stages of the process.
The system generally includes:
- An ozone generator (producing ozone from oxygen)
- Injection or diffusion equipment (to dissolve ozone into water)
- Contact chambers (allowing time for oxidation to occur)
- Off-gas destruct units (safely converting unused ozone back to oxygen)
Once in the water, ozone reacts quickly and aggressively with contaminants.
What makes it unique?
It doesn’t just disinfect—it transforms. Ozone breaks down complex molecules into simpler, more manageable forms, often making downstream treatment more effective or unnecessary.
Where Ozone Fits in Wastewater Treatment
Ozone is typically used as a “finishing tool”—applied after primary and secondary treatment to elevate water quality before discharge or reuse.
Final Disinfection Before Discharge
Meeting discharge limits isn’t optional—it’s regulated and closely monitored.
Ozone provides:
- Rapid inactivation of bacteria and viruses
- Effective disinfection without chlorinated byproducts
- A reliable alternative where chlorine use is restricted
For facilities looking to stay compliant without adding chemical complexity, ozone offers a clean, efficient path forward.
Removal of Pharmaceuticals & Micro-Contaminants
One of the growing challenges in wastewater treatment is dealing with trace contaminants—things like:
- Pharmaceutical residues
- Personal care product compounds
- Hormones and endocrine disruptors
These aren’t always removed through standard treatment processes.
Ozone excels here by:
- Oxidizing complex chemical structures
- Breaking contaminants into less harmful compounds
- Improving overall water quality for discharge or reuse
It’s a forward-looking solution for facilities preparing for tighter environmental standards.
Reduction of Chemical Oxygen Demand (COD)
COD is a key metric in wastewater treatment—it measures the amount of organic material in the water.
High COD levels can:
- Strain biological treatment systems
- Impact discharge compliance
- Increase operational costs
Ozone helps reduce COD by:
- Oxidizing organic matter
- Breaking down stubborn compounds
- Supporting more efficient downstream processing
The result is a more stable, manageable treatment process overall.
Why Facilities Are Integrating Ozone
Wastewater teams are under constant pressure to do more with less—less chemical usage, less environmental impact, and less margin for error.
Ozone helps address those challenges by offering:
- Chemical-Free Oxidation: Reduces reliance on chlorine and other additives
- Advanced Treatment Capability: Targets contaminants traditional systems may miss
- Improved Compliance Confidence: Helps meet evolving discharge regulations
- Operational Efficiency: Enhances overall treatment performance
It’s not just about meeting today’s standards—it’s about being ready for tomorrow’s.
When Timing Gets Tight: How Genemco Supports Your Operation
Even when ozone is clearly the right solution, getting a new system installed isn’t always immediate.
Maybe the equipment is on order…
Maybe the timeline stretched…
Maybe an unexpected issue pushed things forward faster than planned…
Now your team is in a tough spot: you need results now, but your long-term solution is still weeks—or months—away.
That’s where Genemco can help.
Supporting OEMs—Helping You Deliver
If you’re an OEM working with a customer on a new ozone system, we’re not here to compete for that sale.
We want you to succeed—and to be the one who delivers the final solution.
But in the meantime, your customer still has a plant to run and standards to meet.
Genemco can provide available equipment to help bridge that gap:
- A temporary solution to maintain compliance
- A “bandaid” or “tourniquet” to keep operations moving
- A way to support your customer without disrupting your project
When your system is installed, you’re still the hero of the story—we just helped keep things on track.
Image from Genemco
Link to Ozone Systems
Why Teams Lean on Genemco
- Fast Access to Equipment: When waiting isn’t an option
- Cost-Effective Alternatives: Practical solutions for short-term needs
- Real-World Understanding: Experience with industrial and processing environments
- Flexible Approach: Solutions built around your timeline and constraints
The Bottom Line
Wastewater treatment is no longer just about getting through the process—it’s about finishing strong. Removing what others can’t. Meeting standards with confidence. And doing it all efficiently.
Ozone systems offer that extra layer of performance—helping facilities tackle complex contaminants, improve water quality, and stay ahead of regulatory demands.
And when timing becomes the biggest obstacle, having a partner like Genemco can make all the difference.
Because sometimes success isn’t just about the final solution—
it’s about keeping everything running until you get there.