Beneath the surface of every smooth, frozen ice rink is a powerful refrigeration system working to maintain consistent, subfreezing temperatures. Whether it’s a hockey arena, figure skating venue, or community rink, the system’s reliability hinges on several key components—one of the most important being the industrial receiver.
At Genemco, we supply quality used industrial receivers, including brands like RECO and RVS, which are especially known for their durability in demanding, continuous-use environments like commercial ice rinks.
Image from Genemco
Link to Industrial Receivers
What Is an Industrial Receiver?
An industrial receiver is a pressurized storage vessel designed to hold refrigerant within a cooling system. Its primary function is to regulate refrigerant volume and pressure, ensuring smooth and efficient operation. In an ice rink application, this means keeping the ice surface properly frozen and preventing system failure during peak usage.
Why Ice Rinks Depend on Industrial Receivers
Maintaining an ice rink isn’t just about keeping things cold—it’s about delivering precision, consistency, and safety. Here’s how industrial receivers support rink operations:
1. Stabilizing Ice Surface Temperatures
Rinks require a steady refrigerant supply to maintain optimal ice temperatures, typically between 16°F and 24°F. Industrial receivers help by adjusting for refrigerant volume changes, ensuring uninterrupted flow to the evaporators beneath the rink slab. The result? A smooth, reliable skating surface.
2. Managing Variable Loads
Thermal loads at ice rinks fluctuate throughout the day—from resurfacing to games to large events. Industrial receivers absorb and release refrigerant as needed, helping the system adjust without compromising performance or causing pressure spikes.
3. Protecting Equipment
Receivers serve as a protective buffer, ensuring that only vapor enters the compressors. This prevents liquid slugging, which can cause severe mechanical damage. With durable receivers from brands like RECO and RVS, rink operators benefit from reduced maintenance costs and longer system life.
4. Supporting Ammonia-Based Systems
Many ice rinks use ammonia-based refrigeration for its efficiency and low environmental impact. Industrial receivers provide safe refrigerant storage, which is essential for regulatory compliance and operational safety in ammonia systems.
5. Enabling Efficient Maintenance
Industrial receivers make it easier to service and inspect refrigeration systems by allowing portions of the system to be isolated without draining the full refrigerant charge. This flexibility minimizes downtime—especially important during busy skating seasons.
Image from Genemco
Link to Industrial Receivers
Shop Durable Industrial Receivers at Genemco
At Genemco, we understand the unique demands of ice rink refrigeration. That’s why we offer durable, used industrial receivers from proven brands like RECO and RVS—designed to perform reliably in high-capacity, round-the-clock environments.
👉 Browse our inventory today at Genemco.com and find the right receiver to support your facility’s performance, efficiency, and safety.
Need help choosing the right equipment for your rink? Contact Genemco today—our team is here to help you make the best decision for your system and your budget.