How Pet Food Manufacturers Use Industrial Plate Chillers & Freezers

The pet food industry has evolved dramatically in recent years, with growing demand for high-quality, fresh, and protein-rich pet foods. As consumer expectations rise, so does the need for advanced processing equipment—especially when it comes to temperature control.

Industrial plate chillers and freezers play a vital role in pet food manufacturing by helping producers maintain product safety, extend shelf life, and meet strict regulatory standards.

Image from Genemco
Link to Plate Chillers & Freezers

What Are Plate Chillers and Freezers?

  • Plate Chillers rapidly reduce the temperature of liquid or semi-liquid products (such as meat slurries or broths) using stainless steel heat-exchange plates.

  • Plate Freezers press packaged or shaped products between sub-zero metal plates to freeze them quickly and uniformly—ideal for frozen blocks, patties, and pouches.

➡️ Browse Used plate chillers that can be used for pet food manufacturing
➡️ Explore Industrial Refrigeration Equipment


How Plate Chillers & Freezers Are Used in Pet Food Production

🥩 1. Cooling Cooked Meat and Protein Slurries

Many wet and semi-moist pet foods begin with cooked meats, broths, or protein slurries, which must be cooled immediately to prevent bacterial growth.

  • Plate chillers are used to rapidly cool mixtures after thermal processing.

  • This allows the product to move efficiently to the next step: filling, packaging, or further processing.

🐕 2. Freezing Raw and Fresh Pet Foods

With the rise of raw and fresh-frozen pet food, freezing is a critical step:

  • Plate freezers are used to solidify ground meat, fish, or poultry into blocks or trays.

  • They’re also ideal for portion-controlled formats like patties, tubes, or nuggets.

🥫 3. Preserving Nutrient-Enhanced Formulas

High-end pet foods often include added vitamins, probiotics, or raw ingredients that require strict temperature management to retain efficacy.

  • Plate chillers help cool these sensitive components before blending or packaging.

  • For frozen treats, plate freezers offer a compact, efficient way to preserve structure and quality.


Benefits of Plate Chillers & Freezers in Pet Food Manufacturing

  • ✅ Fast Cooling/Freezing: Reduces microbial risk and spoilage

  • ✅ Product Integrity: Maintains structure, color, and nutritional value

  • ✅ Efficient Footprint: High-throughput performance in a compact space

  • ✅ Sanitary Construction: Stainless steel, CIP-ready designs for food-grade use

  • ✅ Regulatory Compliance: Supports FSMA, FDA, and USDA standards for pet food production


Popular Applications

  • Raw & fresh pet food

  • Frozen pet treats

  • Canned food fillers

  • Meat and bone slurries

  • Fish-based or poultry-based formulas

Image from Genemco
Link to Plate Chillers & Freezers


Trusted by Leading Pet Food Producers

At Genemco.com, we provide quality used plate chillers & freezers, and other industrial refrigeration equipment trusted by some of the top names in the pet food industry.


👉 View current inventory of Used Plate Chillers & Freezers