Same Trusted Frick Power, Now Fully Refreshed by Genemco — Rebuilt, Cleaned, Repainted, and Warranty-Backed

At Genemco, pre-owned doesn’t mean second-best. When this Frick RXF-101-H Rotary Screw Compressor Package came through our doors, it already had a strong foundation and the dependable performance Frick is known for. What it needed was expert attention and that’s exactly what we delivered.


 

The Equipment at a Glance

This package includes:

  • Frick RXF-101-H Rotary Screw Compressor

  • Frick XJF151N Motor

  • 250 HP | 460V

  • Frick Micro Control Panel (Quantum HD)

A trusted workhorse in industrial refrigeration systems, this compressor package is designed for demanding ammonia applications where reliability, efficiency, and control matter.

Step One: Deep Inspection & Tear-Down

Every Genemco rebuild starts with a thorough evaluation. Our team inspected the compressor, motor, controls, and vessel to understand its condition and identify what needed attention. From there, the compressor was rebuilt, ensuring critical components met performance and reliability standards.

This isn’t cosmetic work—it’s about extending equipment life and delivering confidence to the next owner.

Step Two: Cleaned, Prepped, and Repainted

Once the mechanical work was complete, the entire package was professionally cleaned and repainted. Beyond looking sharp, repainting helps protect against corrosion and extends service life, especially important in industrial environments.

The result? A compressor package that looks as good as it performs.

Step Three: Tested, Verified, and Backed by Warranty

Before shipment, the unit was reviewed to ensure it was ready for installation and operation. To top it off, this compressor package shipped with a Genemco warranty, giving the buyer added peace of mind.

That’s a key difference when sourcing pre-owned equipment through Genemco—you’re not just buying used, you’re buying refreshed, supported, and ready-to-run.

Same Trusted Frick Power—Refreshed and Ready

The transformation from “before” to “after” tells the story best. What arrived as a used unit left our facility looking renewed, professionally rebuilt, and prepared for years of reliable service.

This Frick RXF-101-H Rotary Screw Compressor Package has officially shipped to its new home, ready to get back to work.


A Trusted Partner for OEMs Facing Long Lead Times

If you’re an OEM or system integrator facing extended lead times on new equipment, Genemco is here to support—not compete with—you. Our goal isn’t to take your sale; it’s to help you protect the relationship and you be the hero for your customer.

Pre-owned, rebuilt equipment like this Frick RXF-101-H can serve as a temporary or interim solution—a reliable bridge that keeps operations running while new equipment is being manufactured and delivered. Think of it as a bandaid or tourniquet solution that buys time without sacrificing performance or safety.

When the new equipment is ready, your customer transitions seamlessly—without downtime, lost production, or strained trust.

👉 View the full listing here:
https://www.genemco.com/products/frick-rxf-101-h-rotary-screw-compressor-package-frick-xjf151n-250-hp-460-v-frick-micro-control-panel-jbs03