Air Cooled Chillers

Air cooled chillers are cooling systems that use air as the medium to dissipate heat from the condenser.

We offer this chiller system from manufacturers like York, McQuay, and Trane.

  • ←
  • →
Frequently Asked Questions

Air-cooled chillers are sophisticated cooling systems that rely on air to remove heat from the condenser. They're commonly used in commercial and industrial settings to maintain a stable temperature and ensure efficient operation of equipment and machinery. These chillers transfer heat from the refrigerant to the air that passes through the condenser coils.

Air-cooled systems are renowned for their reliability and effectiveness in cooling industrial processes and equipment. Unlike traditional liquid-cooled chillers, air-cooled systems utilize the natural cooling properties of air as the primary medium for heat removal. This technology is carefully engineered to efficiently extract heat, guaranteeing optimal performance and durability for various industrial applications. By harnessing the power of air-cooled systems, businesses can achieve precise temperature regulation, mitigating the risk of overheating and maximizing operational efficiency.

Air-cooled systems are essential to many industrial and commercial operations that help maintain optimal temperatures in various settings. These chillers remove heat from a space and release it into the atmosphere through an air-cooled condenser. The process begins with the chiller's refrigeration cycle, where a refrigerant circulates through the evaporator coils, absorbing heat from the building's interior.

As the refrigerant absorbs heat, it transforms into a low-pressure gas and is pumped into the compressor, where it's pressurized and heated. The hot, pressurized gas is then pushed through the condenser coils. Here, the ambient air passes over the coils, dissipating the heat from the refrigerant and causing it to condense back into a high-pressure liquid. The cooled liquid refrigerant is then returned to the evaporator to repeat the cycle and continue cooling the process. The efficient cooling process of air-cooled chillers makes them popular for many applications.

Air-cooled systems offer numerous benefits that make them perfect for cooling systems in various industries. One of the primary advantages of using air-cooled equipment is the energy efficiency. These chillers do not require an external water source for cooling, which eliminates the need for water pumps and cooling towers, resulting in lower energy consumption and operational costs. Additionally, air-cooled equipment is easier to install and maintain than other systems, making them a cost-effective option for businesses looking to streamline their cooling processes.

Another benefit of air chillers is their versatility. They can be installed in various settings, providing flexibility in placement options based on available space and logistical requirements. This flexibility also allows for easy scalability, making it convenient for businesses to expand their cooling capacity as needed. Furthermore, air-cooled units are known for their reliability and durability, ensuring consistent performance and minimal downtime.

Genemco is recognized as a top-tier supplier of pre-owned industrial equipment, including chiller and cooler solutions. Our extensive inventory boasts a wide array of highly-maintained air-cooled chillers sourced from industry-leading brands like York, McQuay, and Trane. What sets Genemco apart is our unwavering dedication to quality assurance. Every chiller in our inventory is meticulously inspected to ensure optimal performance and long-term durability. By prioritizing the highest standards of quality, Genemco guarantees that clients receive cooling solutions that are not only reliable but also aligned with the best practices prevalent in the industry.

At Genemco, we have unrivaled knowledge and deep insight into the industrial equipment sector. Clients who choose Genemco can tap into a wealth of experience accumulated over the years in providing top-notch systems and equipment. This is particularly beneficial for those in food manufacturing facilities and processing plants. Whether you require liquid-cooled chillers or air-cooling systems, partnering with Genemco guarantees that you're obtaining reliable equipment that meets the highest standards in terms of quality and performance. Rest assured that with Genemco by your side, you're making a solid investment in your business's operational efficiency and success.